Browse FAQs

Is a BMXNOR0200H module supported in a M580 Hot Standby system?

Published date: 26 February 2019


Title
BMXNOR0200H and M580 Hot Standby system
 
Issue
BMXNOR0200H and M580 Hot Standby system
 
Product Line
BMXNOR0200H  M580 Hot Standby 
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The BMXNOR0200H is not supported in a M580 Hot Standby system.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.