Technical FAQs

Ask a Question

What is the smallest size motor you can run on the ATV212 or S-F-flex enclosed drive?

Issue:
What is the smallest size motor you can run on the ATV212 or S-F-flex enclosed drive?

Product Line:
ATV21, ATV212 or S-Flex

Environment:
All 

Cause:
run a smaller motor on a larger drive. 

Resolution:
There is no HP setting on the ATV212 drive,  The tHr and F415 motor thermal and motor current settings can be adjusted down to 10% of the drives current ratings.   Keep in mind if they are using a S-Flex enclosed drive with bypass they need to also replace the bypass overload relay to match the smaller full load amps or FLA.
Was this helpful?
What can we do to improve the information ?