Browse FAQs

Preventa XCS Atex_Data sheet of the magnetic switch XCSDMC59030EX

Published date: 06 June 2019

Find attached the XCSDMC59010EX data sheet @, giving the data sheet of the 10m cable length shown in the Osisense Atex Dust documentation. The XCSDMC59030EX magnetic switch, Atex  certified, is a special version having a 30m cable length. It has the same technical data as the XCSDMC59010EX, except 30m cable length. Attached XCSDMC59030EX picture. XCSDMC59030EX part number consists of 2 parts : XCSZC59030EX switch + XCSZC1 magnet. The XCSZC59030EX reference is not sold separately
http://www.tesensors.com/global/en/product/safety-switches/atex-preventa-xcs-ref/?cat_id=BU_AUT_2224_L3&conf=sensors&el_typ=product&prd_id=XCSDMC59010EX&scp_id=Z000

Was this helpful?

What can we do to improve the information ?