Technical FAQs

Ask a Question

What is the reason that TeSys GV range Icu (kA) decreases with increase in motor kW rating.


The internal impedance of the product decreases when the rating of the GV increases. With a reduced impedance, the limitation of overcurrent (including short-circuit level) decreases. 

 
Was this helpful?
What can we do to improve the information ?