Technical FAQs

Ask a Question

ATV212HD75N4- What is the maximum Continuous output current of this drive?

Issue:
How do I find the maximum continuous output current rating of a drive?

Product Line:
All Altivar drives 

Environment:
All

Cause:
Clarification of published information.

Resolution:
In the installation manual for each drive family, there will be a Drive Ratings table.  Among other information, the Nominal Output Current is listed for each drive part number.  This rating is also the maximum continuous output current rating of the drive.   The drive may be able to operate above this level for short duration only, as listed in the Max Transient Current column of the drive ratings table.
Was this helpful?
What can we do to improve the information ?