Technical FAQs

Ask a Question

The Opening / Closing orders on the Compact NSX motor mechanism can be impulse or maintained type?

The opening and closing orders on the Compact NSX motor mechanisms can be either impulse or maintained type.
Very important is not to give the opening and closing order at the same time, because then the motor mechanism enters in an endless cycle which may damage it.
Was this helpful?
What can we do to improve the information ?