Technical FAQs

Ask a Question

How to calculate the long time pick-up (Ir) of CVS 630 equipped with TM600D?

The In value for breaker CVS630 (equipped with TM600D) is given as 600A as per the trip unit rating.
Therefore, when we say Ir setting is from 0.7 to 1 x In, here In is the trip unit rating.


 
Was this helpful?
What can we do to improve the information ?