Technical FAQs

Ask a Question

Power Monitoring Expert 8.2: How to perform a Logical Device Import for the EM4900 device driver?

Issue
Customer encounters issues when importing the EM4900_Logical_Device.csv as described in the EM4900 SE Driver Release Notes.pdf. 

Product Line
Power Monitoring Expert 8.2

Environment
Device driver installation

Cause
The EM4900 SE Driver Release Notes.pdf contains several misprints that will cause the logical device import to fail.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).​

In the example below, the EM4900_Logical_Device.csv will be modified per the following customer criteria
  • to reference a physical device named Building1.EM4900
  • to create a single Logical Device named Building1.Meter_A
  • using the logical device type previously created per EM4900 SE Drive Release Notes.pdf called EM4900 Logical Device
 
  1. Open EM4900_Logical_Device.csv using Excel
Original EM4900_Logical_Device.csv
 
  1. Update the following:
  • Replace each circuit name in column A with meaningful logical device name in group.name format
  • Delete any unwanted rows
  • Replace the entire column B with the name of the logical device type that was given to the logical device type in the Logical Device Type Editor
  • Replace all the cells in column C with the device name entered in Management Console
  • Confirm all the cells in column D at set to EM4900 as this is the physical device type specified in Management Console
  • Replace the placeholder in "@<physical meter name>_Px_Mxx" with the physical meter name
For example, alter "Demand Current Avg - Sliding@EM.EM4900_P1_M01"
to be "Demand Current Avg - Sliding@Building1.EM4900_P1_M01".
  1. Import the file from Management Console (Tools > Logical Device > Import Logical Device)
 
Edited EM4900_Logical_Device.csv
 
 
Was this helpful?
What can we do to improve the information ?