Technical FAQs

Ask a Question

How to modify the default PC-based logging for an ION6200 when it is communicating over Modbus or ION protocol?

Issue
The ION6200 is not capable of onboard logging. Therefore, the customer would like to know how to modify the default PC-based logging for the ION6200 in Power Monitoring Expert.

Product Line
ION6200

Environment
Power Monitoring Expert 8.x

Cause
The ION6200 does not contain onboard data logs. Therefore, all logging is specified in the device driver regardless of the protocol being used.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).
  1. Open Management Console
  2. Select Tools > System > Modbus Device Importer 
  1. In the Modbus Device Importer, select File > Open
  2. Navigate to \Power Monitoring Expert\system\translators
  3. Open the file, 6200.ion 
  4. Select Configure Logging and Calculation 
 
  1. Make the desired modifications
  2. Click OK 
  3. Select File > Save 
  4. Select Tools > Update Device Type 
  5. Exit the Modbus Device Importer 
Was this helpful?
What can we do to improve the information ?