Technical FAQs

Ask a Question

Are pins 17 and 19 and also 18 and 20 of the BMXDAI1604 internally connected?

Pins 17 and 19 of the BMXDAI1604 input module are internally connected. Pins 18 and 20 are also internally connected.
Was this helpful?
What can we do to improve the information ?