Technical FAQs

Ask a Question

Is there a replacement for the TWDXCPMFK64 memory cartridge?

There is no replacement for the TWDXCPMFK64 memory cartridge.

- TWDXCPMFK64 is part of the Twido line of controller which at this point is obsolete.
- The replacement for the Twido controllers are the M221 controllers. All M221 controllers have a SD card that can be used to transfer a program or backup an application and 2MB of flash memory.
- A customer looking for a TWDXCPMFK64 should be looking into converting his Twido project to a M221 / SoMachine Basic project. A Twidosuite project can be opened and converted easily into a SoMachine Basic project.
- Please contact the automation technical support at 888-266-8705 if you need to convert a Twido controller to a M221 controller
Was this helpful?
What can we do to improve the information ?