Browse FAQs

How to upgrade a Distributed Installation of ENM 8.x to a Distributed Installation ENM 8.3.3/8.3.4

Published date: 20 December 2018

Issue
The Event Notification Module Installation Guide does not specifically address upgrading distributed installations.

Environment
Distributed installation of Event Notification Module 8.x

Resolution
  1. Uninstall ENM 8.x on both the Application and Database server through the Control Panel > Programs and Features.
  1. Install ENM 8.3.3/8.3.4 on the Database server by running the install executable, MainSetup.exe.
When prompted, select a Setup Type of Event Notification Module - Database Server
 
  1. Install ENM 8.3.3/8.3.4 on the Application server by running the install executable, MainSetup.exe.
When prompted, select a Setup Type of Event Notification Module - Application Server
 


The ENM 8.3.3 Installation Guide can be found in FA338107.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.