Technical FAQs

Ask a Question

Do you need to access the web page to set up the ATV630 and ATV930 drives to work with Ethernet IP assemblies?

Issue:
Do you need to access the web page to set up the ATV630 and ATV930 drives to work with Ethernet IP assemblies?

Product Line:
Atlviar ATV630 and ATV930 drives. 

Environment:
All 

Cause:
Needs to  use  Somove to set up the drive

Resolution:

You don't need the web page to set up the drive you will need to download somove and the DTMs to connect and set up the drive. 

You will will need to download somove and the DTM files to set up the ATV930 drives.. 

You can use your Ethernet cable to connect to the drive and somove. 

Somove 
https://www.schneider-electric.com/en/download/document/SoMove_FDT/ 


DTM files 9XX drives 
https://www.schneider-electric.us/en/download/document/ATV9xx_DTM_Library_EN/ 


DTM files for 6xx drives 
https://www.schneider-electric.com/en/download/document/ATV6xx_DTM_Library_EN/ 


DTM for Altivar drives in General 
https://www.schneider-electric.com/en/download/document/Altivar_DTM_Library/ 

You can use a standard Ethernet cable or the TCSMCNAM3M002P cable.  
Was this helpful?
What can we do to improve the information ?