Browse FAQs

Video: What is the difference between Target and Panel Function Keys in Vijeo Designer?

Published date: 15 November 2018

Issue:
Understanding the differences between Target and Panel Function Keys.

Product Line
XBTGK and HMIGK series
XBTF series 

Environment:
Vijeo Designer
XBTL1000

Resolution:
  • Target Function Keys (Formally called Static Function Keys in the XBTL1000 software)
    • Same function regardless of the active panel.
 
  • Panel Function Keys (Formally called Dynamic Function Keys in the XBTL1000 software)
    • Different function depending on the active panel.

The following video demonstrates process of configuring the Panel and Target Function Keys on a Magelis HMIGK Touch screen Panel with Keypad via Vijeo Designer version 6.2:

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.