Technical FAQs

Ask a Question

What are the mounting positions for a Masterpact NT/NW Breaker?

It is important to distribute the weight of the device uniformily over a rigid mounting surface such as rails or a base plate. This mounting plane should be perfectly flat (tolerance on support flatness: 2 mm). This eliminates any risk of deformation which could interfere with correct operation of the circuit breaker. Masterpact devices can also be mounted on a vertical plane using the special brackets.

Mounting options available for this range are depicted in the extract from the Masterpact NT and NW catalogue

Top Level > Product Category > Buildings & IT > Partner Project Transactional > Air Circuit Breakers > ACB NW08/50 (B2-ANSI)
Was this helpful?
What can we do to improve the information ?