Technical FAQs

Ask a Question

How can I activate SNTP in Easergy P3?

You need to set the IP address for your SNTP server under protocol configuration. There are two IP addresses, main and backup. The device will initially connect to the main server and if connection is lost device will automatically connect to the backup server.
 
Was this helpful?
What can we do to improve the information ?