Technical FAQs

Ask a Question

How do I know if the Easergy P3 device receive selected synchronisation?

From HMI, scroll down to menu CONF, then press arrow right until you reach menu CLOCK SYNC. The parameter SySrc show the active synchronisation method. In case the value is “Internal” no synchronisation source is received.

From eSetup Easergy Pro you can find same information under General/Clock sync
Was this helpful?
What can we do to improve the information ?