Technical FAQs

Ask a Question

Can DNP3 Master Output Data be resent manually with a BMXNOR0200H module?

Title
BMXNOR0200H DNP3 Master Output Data
 
Issue
Resending BMXNOR0200H DNP3 Master Output Data
 
Product Line
BMXNOR0200H
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 There is no way to manually resend the DNP3 output data from the BMXNOR0200H module setup as a DNP3 Master.
The only way to have the DNP3 Master message resent is to increase the number of retries.  
For more information, reference the BMXNOR0200H module Channel and Session Advanced parameters on pages 277 and 279 in the user manual.

 
Was this helpful?
What can we do to improve the information ?