Technical FAQs

Ask a Question

Can I also use a serial protocol at the same time with Ethernet protocols?

 Yes, if the hardware support serial port you can also use e.g. Modbus/RTU or other serial protocol at the same time.
Was this helpful?
What can we do to improve the information ?