Technical FAQs

Ask a Question

Can I use both IEC61850 some other Ethernet protocol like DNP or Modbus at the same time?

 Yes, two Ethernet protocols can be defined simultaneously
Was this helpful?
What can we do to improve the information ?