Technical FAQs

Ask a Question

Can I get fault values when using IEC61850 communication

Yes, Logical Nodes IOC1GGIO142, IOC2GGIO143 and IOC1GGIO144 include the fault currents of each overcurrent stage.
Was this helpful?
What can we do to improve the information ?