Technical FAQs

Ask a Question

I cannot find protection function signals like TRIP or START in GOOSE dataset, how can I publish such signals?

You need to create the signal using logic. E.g. below the first stage overcurrent trip is published as logic output 3
See example in attachment.
Was this helpful?
What can we do to improve the information ?