Technical FAQs

Ask a Question

Does Easergy P3 support Profibus?

Yes, P3 support Profibus DP with external accessory REL52815 (VPA3CGSE)
In order to connect external accessory REL52815 (VPA3CGSE) to P3 standard you need a communication card with serial port and the cable REL52827(VX084). For the power supply to VPA you need to connect external 12 Vdc to the cable. In P3 advanced, you need a communication card with serial port and the cable REL52824 (VX072). No additional power supply needed.
Was this helpful?
What can we do to improve the information ?