Technical FAQs

Ask a Question

Why can’t I add IoCalc to the recorder channels?

 Calculated values can only be added to recorder channels if the trend mode is selected, e.g. 1/10.
Was this helpful?
What can we do to improve the information ?