Technical FAQs

Ask a Question

What are the eight programmable stages used for?

 The stages can be used to extend your protection functions or add more stages. You can freely select an analogue measurement to be coupled to the stage, set comparision condition and then set a threshold for the comparision. The programmable stages can be connected to ouputs in output matrix
Was this helpful?
What can we do to improve the information ?