Technical FAQs

Ask a Question

When I connect the value to mA output it seems not to change value in VIO module?

You must write x1000 to the module. For 4-20 mA, you should then define Modbus Min to 4000 and Modbus Max to 20000

Was this helpful?
What can we do to improve the information ?