Technical FAQs

Ask a Question

If the block signal is released, will the function activate or will the timer be reset?

 Block matrix will only block when signal is active, in case the signal is released the function will activate. Timer is not reset from block function.
Was this helpful?
What can we do to improve the information ?