Technical FAQs

Ask a Question

Do I need to activate separately each protection stage in order to get an activation?

Yes, each stage need to be set to enable in order to get an activation for reaching the threshold in the “Valid protection stages” menu. The same setting is also available in each protection stage menu.

Was this helpful?
What can we do to improve the information ?