Technical FAQs

Ask a Question

My device only have one voltage input, will the adaptation of frequency still be from that voltage input?

No, In case the device only have one voltage input the frequency adaptation is taken from measured currents. 
Was this helpful?
What can we do to improve the information ?