Technical FAQs

Ask a Question

Why can I only see 5A as nominal input for phase currents

The device CT hardware inputs are calibrated to 5A nominal but you can connect an 1A phase CT to the same inputs. The CT secondary can be scaled between 1 – 10A
 
Was this helpful?
What can we do to improve the information ?