Technical FAQs

Ask a Question

I cannot select the object on LCD in order to do a control

Check that the Object open and close signals are mapped to outputs in Output matrix. Only such objects can be selected on LCD for control.

Was this helpful?
What can we do to improve the information ?