Technical FAQs

Ask a Question

If I connect with USB serial connection, do I need to consider the communication speed?

 Yes, please check / change speed setting from HMI. Scroll with arrow down until you reach “CONF” menu. The first row show the speed setting for front port.
Was this helpful?
What can we do to improve the information ?