Browse FAQs

What is the maximum length that my Bacnet network cable can span on the ATV600 series drives?

Published date: 20 August 2019

Issue:
Maximum length that my Bacnet network cable can span on the ATV600 series drives.

Product Line:
ATV600 series drives with VW3A3725 Bacnet option card.

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:
Cable lengths of up to 1200 m (4000 ft.) daisy chained from device to device are supported.  A signal repeater is required after 1200 m (4000 ft) to add more nodes to the network or further extend the cabling.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.