Technical FAQs

Ask a Question

What is the unit load of the VW3A3725 Bacnet option card for the ATV600 series drive?

Issue:
What is the unit load of the VW3A3725 Bacnet option card for the ATV600 series drive?

Product Line:
VW3A3725 Bacnet MS/TP option card.

Environment:
All models, All serial numbers.

Cause:
Clarification

Resolution:
The unit load of the VW3A3725 Bacnet Option card is 0.5 Unit Load.
Was this helpful?
What can we do to improve the information ?