Technical FAQs

Ask a Question

Why Ecodial restricts Maximum Cable Cross Section Area to 300 Sq.mm in project parameters tab as well as in the individual cable properties tab in Ecodial Advance Calculation?

Ecodial Advance Calculation have restricted maximum cable cross section to 300Sq.mm in the project parametrs tab but in the manual choice controller its possible to select upto 1000Sq.mm
1. As per the IEC standard, most of the cable installation method (except 2 or 3 installation method)  the maximum cable cross sectoion area is restricted to 300Sq.mm. so to obey the IEC guidelines, in the project parameters it is restricted to 300Sq.mm. Ecodial always suggests the cable Cross Section Area in-line with above restriction.
2. But in the market, more than 300Sq.mm cables are available and to help the customer in getting the calculation and solution for more than 300Sq.mm cross section area (upto 1000Sq.mm) cables we have provided the option of selecting it in the manual choice controller. 
Was this helpful?
What can we do to improve the information ?