Technical FAQs

Ask a Question

Is there any logical improvement to find a PFC solution based on the pollution level in Ecodial Advance Calculation?

From onwards EAC 4.8.6 INT, Logical implementation is made available to find a PFC solution based on the pollution level (harmonic disturbance) of the network.
Gh/Sn = 0 to 14 %No Pollution 
Gh/Sn =15 to 24%Low Pollution 
Gh/Sn = 25 and above Polluted
Was this helpful?
What can we do to improve the information ?