Technical FAQs

Ask a Question

What temperature derating has to be applied on the iC60 RCBO devices?

On the iC60 RCBO the following derating needs to be applied depending on the ambient temperature.



* More technical parameters about the iC60 RCBO in the catalog pages under the code CA902044E.
Was this helpful?
What can we do to improve the information ?