Browse FAQs

Osisense XC - Adapted XCKJ10513H29S89 limit switch data sheet

Published date: 06 June 2019

The adapted limit switch XCKJ10513H29S89 is exactly the same as the standard product XCKJ10513H29 (same data sheet). XCKJ10513H29S89 complete switch = ZCKJ1H29 body + ZCKE05 head + adapted ZCKY13S89 roller lever. The adapted ZCKY13S89 roller is based on the standard ZCKY13 steel roller lever. The adaptation consists of punching the centre of the axle in order to avoid the loosening of the nut. Please look at the picture showing the concerned axle.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.