Technical FAQs

Ask a Question

Is it possible to apply fault reset on ATV320 and ATV340 via STOP/RESET key on HMI?

VW3A1111 keypad has not been developed and validated for ATV320. Hence, VW3A1111 isn’t compatible with ATV320 (and legacy drives). 
For ATV320, VW3A1101, VW3A1006 and VW3A1007 keypad are the only keypad compatibles.
Fault reset from these pannels is possible if the panel is selected as active control channel. HMI must be active Freq reference channel ((in not separate mode) or active command channel (in separate mode)
For ATV340 likewise, it is possible to apply fault reset from VW3A1113 if the HMI is active control channel.
Was this helpful?
What can we do to improve the information ?