Technical FAQs

Ask a Question

New Alarm Tags in SCADA don't Show in ENM

Issue
New alarm tags were added to PowerSCADA Expert (PSE).  However, when configuring Event Notification Module (ENM), the tags are not transferred.

Product Line
Event Notification Module

Environment
ENM setup screen

Cause
The Core Servive Host is responsible for synchronizing PSE and ENM.  This issue happens when syncronization does not take effect between PSE and ENM.

Resolution
The CoreServiceHost needs to be stopped and started again (a restart may not work):
1. Stop Schneider Electric CoreServiceHost in Services
2. Start Schneider Electric CoreServiceHost in Services.
Was this helpful?
What can we do to improve the information ?