Technical FAQs

Ask a Question

Is there a way to determine if the 140CRP93x 00 or 140CRA93x 00 is RoHS or Non RoHS compliant?


 

           Non  RoHS                                          RoHS

  140CRP93X 00 <= PV07   Non RoHS                   140CRP93X 00  => PV08   RoHS
  140CRA93X 00 <= PV08   Non RoHS                   140CRA93X 00  => PV09   RoHS

  If there are no PV designations on the CRP or CRA, the products should be considered Non RoHS. 


R-122018


 

  
Was this helpful?
What can we do to improve the information ?