Technical FAQs

Ask a Question

What are the default serial port settings in Em64xxH series meter ?

The meter is factory-configured with the following default serial communications settings:

• Protocol = Modbus RTU
• Address = 1
• Baud rate = 19200
• Parity = Even
Was this helpful?
What can we do to improve the information ?