Technical FAQs

Ask a Question

What is the maximum energy value available in EM64xxH series meter ?

Energy readings of the power meter will overflow when either Delivered (Utility), or
Delivered (Alternate Source), or Total (Utility + Alternate Source) energy reaches
99,999.999 G. This depends on PT (VT) and CT ratios programmed in the meter.
Was this helpful?
What can we do to improve the information ?