Technical FAQs

Ask a Question

Osisense XM - Is our XMLR pressure transmitter compatible with kerosene fuel to control

1) Kerosene fuel is considered as Fuel oil n°1 or Aircraft fuel in the ATEX standards. It is classified in temperature class T3. So to control such explosive liquid, you need to use an Atex Gas pressure transmitter or pressure switch certified for such use.
2) Our electronic pressure sensors (XMLR, XMLP, XMLK, XMEP ...) and our electromechanical pressure switches XMLA/B/C/D or ACW/ADW ... are not suitable for such use, they are not Atex Gas certified.

Was this helpful?
What can we do to improve the information ?