Technical FAQs

Ask a Question

What is the output frequency range of an ATV312 drive?

Issue:
What is the output frequency range of an ATV312 drive?

Product Line:
Altivar 312 drives

Environment:
All

Cause:
N/A

Resolution:
The output frequency range of the ATV312 drive is 0...500 kHz.

 
Was this helpful?
What can we do to improve the information ?