Technical FAQs

Ask a Question

NOE kernel update

 Goals and Symptoms
 
How to upgrade an old NOE kernel?
                    
Facts and Changes
 
Quantum, 140NOE771**
 
Causes and Fixes
The Kernel version is available in the the properties of the NOE from the embedded webpage or the EXECLoader can be used for that purpose.

The Kernel can not be download via FTP, the EXECLoader is needed; that tool comes with Concept or Proworks32 as a bundle, not separated.

 
Concept can be found at http://shoppingkiosk.schneider-electric.com/doc_info.aspx?DocRef=PRMALLIANCE00078&isdvd=False&df=12&gid=424621#

Here is the procedure to upgrade the NOE Kernel, extracted from Unity pro help.
 
Was this helpful?
What can we do to improve the information ?