Technical FAQs

Ask a Question

The Micrologic 2.2M and 2.3M can be used on 400Hz?

Yes, the Micrologic 2.2 M and 2.3M can be used on 400Hz application. The same thermal derating has to be applied as published in the catalog for the other Micrologics (attached file).
Was this helpful?
What can we do to improve the information ?