Technical FAQs

Ask a Question

Ecodial advance Calculation is not automatically proposing upstream protection device for UPS Galaxy 300, 1X30KVA. How can I select suitable protection device?

Yes. Ecodial Advance Calculation is not automatically proposing upstream protection device for 1X30KVA Galaxy 300UPS.
Follow the below steps to selct protection device manually
1. Click on the manual choice controller of upstream protection device 
2. Select the breaker Acti 9 C120H/D 80A as manual choice
3 Now Ecodial will calculate the network smoothly
Was this helpful?
What can we do to improve the information ?