Technical FAQs

Ask a Question

Why downstream cable cross section are not displaying on network/properties tab solution section for ATV 320, 630, 930 Variable Speed Drives in Ecodial Advance Calculation?

Currently Ecodial Advance Calculation database do not have downstream Cable cross section area  database for ATV 320, 630,930 range variable speed drives. That is the reason Ecodial Advance Calcdoes not proposes the Downstream CSA value.
Was this helpful?
What can we do to improve the information ?