Technical FAQs

Ask a Question

In Ecodial Advance Calculation, for outdoor application (IP 68) Transmission busways are available?

Canalis KR is available after the selection of "Outdoor IP68" for "Required IP" option in the Properties tab.
KRA - available as solution for the selection of Conductor metal of phase as Aluminum
KRC - available as solution for the selection of Conductor metal of phase as Copper
Was this helpful?
What can we do to improve the information ?